REGEN.REXT

Description

REGEN.REXT sets the external user-defined regen resistor resistance. This variable is needed for the regen resistor temperature estimation algorithm.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Ω

Range

0 to 330 Ω

Default Value

330 Ω

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.REXT

3007h

06h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.REXT

2401

961

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.REXT

2401

Unsigned16

Read/Write

-